AXIS#.DBILIMITACTUAL

Description

This parameter returns the minimum value of the following parameters: AXIS#.DBILIMIT , AXIS#.ICONT , AXIS#.MOTOR.ICONT .

Example

Assume AXIS1.ICONT = 3 Arms, AXIS1.DBILIMIT = 1 Arms, and AXIS1.MOTOR.ICONT = 2 Arms. Then AXIS#.DBILIMITACTUAL will return 1 Arms.

Versions

Action Version Notes
Implemented 02-07-00-000

General Information

Type

Read only

Description

Returns the minimum value of the AXIS#.DBILIMIT , AXIS#.ICONT , AXIS#.MOTOR.ICONT keywords.

Units

Arms

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.DBILIMITACTUAL

5000h

11h

Unsigned32

-

1000:1

Read only

No

AXIS2.DBILIMITACTUAL

5100h

11h

Unsigned32

-

1000:1

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.DBILIMITACTUAL

5035

13AB

Unsigned32

Read Only

-

AXIS2.DBILIMITACTUAL

70571

113A

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.DBILIMITACTUAL

5035

Float

Read Only

-